STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

delay inside a EXTI9_5 callback function

I have been trying to create a asynchronous serial UART communication on GPIOA pin 9 and pin 8pin9- is RxPin8- is Txin order to sample the message at the right time I have create a dealy function using the DWT mechanism, the idea is to wait 1.5*(1/b...

FDCAN Arbitration lost / LEC error doesn't handled with IRQ in DAR mode. Probably - the potential hardware bug.

Hello guys.I try to catch the IRQ of arbitration lost and error code in LEC in FDCAN in DAR (disabled auto retransmission) mode.I have 3 devices in CAN network:   STM32F207 - 2 pcs   STM32H745Q (dev board) + external phy.All devices works good. They ...

SPI Tsize-Tser

Hello , ı read RM0433 ,I could not understand the process in the image below(page 2198)

0693W00000JNrN5QAL.png

Resolved! Nucleo L476RG - Turn on LED

I am using a NUCLEO-L476RG development board, I am learning to write GPIO drivers for STM32 family I am implementing a simple logic in which I need to turn on an LED when a push button is pressed.I have a strange issue: The Bread board LED turns ON w...

0693W00000JNq9WQAT.png
Tbone1 by Associate II
  • 5230 Views
  • 8 replies
  • 0 kudos

How to convert old code to use FPU ?

Hi I am trying to optimise my gait generation code for my robot. I use a lot of float operations . I want to use FPU to accelerate computing. As an experiment I am using the following taskTickType_t start = xTaskGetTickCount(); while( i<100000000) ...

0693W00000JMnPeQAL.png
SSRIN.1 by Associate III
  • 3986 Views
  • 7 replies
  • 0 kudos

Would it be possible to calibrate the M48T12 memory using an STM32?

Hello,The M48T12 memory outputs a test signal at 512Hz, with a deviation of 0.001Hz.I tried to read this deviation using a 24MHz sampling logic analyzer, but there was still a fluctuation in the reading of the thousandths of a Hz.I think maybe a 100M...

by Not applicable
  • 2992 Views
  • 7 replies
  • 0 kudos

NOR flash mass erase hangs STM32H753?

Just got a weird problem with a NOR flash, memory mapped on FMC, address 0x60000000.The model is IS29GL128, 16 MB. Most of the code borrowed from eval. board examples.Basically it works (write, read, erase). But during mass erase the systick interrup...

Pavel A. by Super User
  • 1667 Views
  • 2 replies
  • 0 kudos

Resolved! Same codebase across multiple projects

HelloI'm using STM32cubeide with STM32LI have several applications that are based on the same code base.What are the good solution(s) to handle this common code with stm32cubeide?I can consider several solutions, one application = one project or one ...

po221 by Senior
  • 3412 Views
  • 7 replies
  • 0 kudos