STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to find where RXNEIE is reset to 0

Hello,I'm debuging some legacy code for an STM32L476RG MCU. USART2 is enabled, and used as an UART, with DMA for TX, and one interrupt per received character. I'm using STM32CubeIDE 1.8.0.Each time a character is received, the HAL_UART_RxCpltCallback...

wake up logic on stm32l4

I want to wake up from standby for each transition on a wkup pin. For example, on waking, read the wakup pin and set/reset the bit in pwr_cr4.  (pin high -> bit high, pin low -> bit low).  Is there a race condition ?  The reference manual is vague on...

I2C Master Sequential function

Dear,I currently use a STM32G070 with external touch sensor component usuing I2C interface.This component aloow me to communicate with it only during a ready window and this window is automatically closed after a delay without communication or a I2C ...

0693W00000JPpzuQAD.png
YDann.7 by Associate III
  • 6606 Views
  • 5 replies
  • 0 kudos

Can sdio f_mount affect UART port?

Hi!I have a problem with the simultaneous use of an SD card (with SDIO) and the uart port with GSM module connected. The SD card works flawlessly all the time. Communication with the GSM module is very unstable when I use the SD card - using the f_mo...