cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G030K6Tx: configuring HSE crystal

mgrnr80
Associate

With STM32CubeIDE there is only one option to configure HSE clock, i.e. BYPASS Clock Source, how to configure a crystal resonator?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Hello

As i can see from Datasheet for LQPF32 there is not any OSC_OUT pin ,

STM32CubeIDE gives only this option because the absense of OSC_OUT pin ,

Bowman32
ST Employee

Hi @mgrnr80​ 

You can refer to STM32G030x6 datasheet DS12991 Rev 3 table 12 Pin assignment and description.

For LQFP32 package you can only use HSE in bypass mode but with LQFP48 package you can use HSE crystal mode.

Also, you can refer to reference manual RM0454 Rev 5 section 5.2.1 HSE clock

Please mark my answer as best by clicking on the "Select as Best" button if it fully answer you question. This will help other users to find it more quickly.

Bouraoui

Am I missing something? According to STM320G0x6 datasheet there's OSC32_IN(PC14) and OSC32_OUT(PC15) pins.

So, how can't we configure HSE clock?

waclawek.jan
Super User

> OSC32_IN(PC14) and OSC32_OUT(PC15) pins

These are related to LSE, not to HSE.

JW