cancel
Showing results for 
Search instead for 
Did you mean: 

USB virtual com port can't receive data when device reboot

hjuns
Associate III

Hello,

I experienced a phenomenon in which the USB port was not reconnected.

This phenomenon occurs when a USB port is connected to the product and reboots.

0693W00000Dmc7wQAB.pngI check my device manager.

When i turn off product, com port also disappear.

and product reboot then com port appear.

But i can't receive any data.

When i reconnect USB cable then communication work well.

Summary

  1. USB virtual com port can't receive data when device reboot.
  2. In the same state as above, USB cable reconnect then USB connect well.

I need your support.

Thanks. best regards.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
hjuns
Associate III

I solved this problem.

It need USB gpio pull down.

If device restart then USB gpio pull down.

View solution in original post

4 REPLIES 4
Pavel A.
Super User

After the device restarts, do you see the enumeration process? If not, it's the time to unpack your USB bus analyzer,

hjuns
Associate III

I solved this problem.

It need USB gpio pull down.

If device restart then USB gpio pull down.

TDK
Super User

Huh? What is a USB gpio pull down?

If you feel a post has answered your question, please click "Accept as Solution".
hjuns
Associate III

USB_OTG_FS_DM, USB_OTG_FS_DP need pull down.