STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5 Backup SRAM in standby

Hi,I have a question regarding the backup SRAM in the STM32U5. The reference manual is not clear about this:On the one had, it mentions the following Which seems to indicate that it is possible to place the device in standby without powering SRAM2. H...

ArnoutDekimo_0-1715695675370.png ArnoutDekimo_1-1715695729787.png ArnoutDekimo_2-1715695838490.png

Resolved! STM32H753 SPI Transmission

Hi, I'm using the STM32H753-NUCLEO Board for some SW development, and I'm having some issues with the SPI Handling.I'm attempting to transmit a single 16-bit data packet, however on the scope I'm transmitting two 16-bit data packets. When I change my...

Resolved! USB composite CDC+UVC stops receiving data on EP

HiI created a composite USB device with CDC and UVC classes using usbd. The device is detected, camera image streaming works, and data transfer via CDC (virtual serial port) also works. However, after a random time, communication on the CDC data out ...

Artur5 by Associate III
  • 993 Views
  • 2 replies
  • 1 kudos

Resolved! Hard Fault Unaligned Error on memory region from SDRAM

Hi everyone! I have a working project based on STM32F746 with LCD, Ethernet and SDRAM(IS42S16160J-6TL) and now we are moving it to STM32H753II. I set up a FMC controller and tested whole SDRAM region with 8, 16, and 32 bit access. I use GCC. During t...

Zed by Associate III
  • 1513 Views
  • 5 replies
  • 2 kudos