cancel
Showing results for 
Search instead for 
Did you mean: 

SDMMC and USB Mass Storage Class (MSC).

indhuja
Associate

I am using the STM32H745I-DISCO board, where Core M4 handles SDMMC and FATFS, and Core M7 manages USB Mass Storage Class (MSC). Is there a procedure or any available documentation on linking both cores for seamless data sharing?

3 REPLIES 3
Pavel A.
Super User

Sharing which data? Do you mean, sharing the filesystem on SD card between the CM4 and CM4 applications? (like, both CM4 and CM7 can create files on the SDcard?)

 

indhuja
Associate

No. File system should create in m4 , Only file access needs to be implemented in USB.

1. Write all sensor data in flash through m4.

2. Collect stored data through M7 via USB mass storage

Very good, so the CM4 and CM7 just need to send data between them. Use any internal RAM that can be shared between them, and hardware semaphores for synchronization.