Question
STM32H745IIK6 GPIO Pxx_C pin configrations
On our custom board using STMH745IIK6 we cant use both PC3_C and PC3 pins together. PC3 is configured as ADC reading 1.7V and PC3_C is configured as SPI MISO and when configured this way we cant read SPI device (I3G4250D) also ADC reads corrupt as well. When using only ADC we can read the correct readings but still we cant read SPI device when closing the ADC port.
Is there any way we can switch between this pins?
Are we missing any critical points when using this pins ?
Thank you,
Ali.