User Activity

Hi,I tried booting the STM32F103C8T6 via UART following the boot configuration details from the AN2606 document provided by ST. I have outlined the configuration below.After setting up the boot configuration, I attempted to connect the STM32's UART u...
Hello STM32 Community,I am currently working on a USB Power Delivery (USB PD) project using an STM32L562CET6 microcontroller, where I successfully vary the output voltages and currents (5V 3A, 9V 3A, 12V 3A, 15V 3A, and 20V 5A) in SPR (Standard Power...
I want to create USB PD Sink Demo on STM32L562CET6, i referred the below demo.LINK Below:STM32L562 EDK USB PD Demo from STM32 is that possible recreate the same demo to the STM32L562CET6 or any changes need to be do because i didn't get any output vo...
Title:"Demo for STM32L562 with BQ25756 Charger Controller?"Hello STM32 Community,I am currently working on a project involving the STM32L562 microcontroller and the BQ25756 battery charger controller. I am looking for a demo or example project that d...
Kudos given to