Skip to main content
Associate II
January 30, 2025
Question

Unable to Debug or Connect STM32L562E-DK After Enabling Read Protection

  • January 30, 2025
  • 4 replies
  • 633 views

Hi,
I am facing an issue with my STM32L562E-DK board. Initially, I was able to debug it using STM32CubeIDE. However, after attempting to configure the controller in UART boot mode, I accidentally enabled read protection (DC:LEVEL 1). Since then, I cannot debug the board or connect to it using STM32CubeProgrammer.

Whenever I try to connect the controller via STM32CubeProgrammer, it fails to establish a connection. I suspect something went wrong during the configuration.

I have attached an image below showing the error that occurs when I try to connect.

Screenshot 2025-01-30 174748.png

How can I resolve this issue and regain access to my controller?

Edited by ST Moderator to correct the board name STM32L562E-DK (instead STM32L62E-DK)

This topic has been closed for replies.

4 replies

ST Employee
January 30, 2025

Hello @Sankar_Eswaran ,

connect using the hotplug mode in CubeProgrammer .
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
January 31, 2025

Hi,

i tried every mode but it still not connecting is there any specific documents steps need to be follow ?

Screenshot 2025-01-31 112608.png

 

Thanks & Regards 

Sankar Eswaran.

Visitor II
March 21, 2025

Hello, I also encountered the same problem after modifying RDP. I am also using the stm32l56e-dk board. Can you successfully connect to this board?

ST Technical Moderator
January 31, 2025

Hello @Sankar_Eswaran ,

Did you try connecting under reset? Once connected, perform a mass erase to remove the read protection.

Try using the ST-LINK for debugging only and use another power supply source. Apply a power off/on cycle while the ST-LINK USB cable is already plugged in. After that, the tool should be able to connect to the target and launch RDP regression.

Please refer to this article, this will help you What option bytes in STM32 are, and how to use the... - STMicroelectronics Community

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks