STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Send COMP output to 2 TIMs as follower and inverter.

I want to generate differential signal from this MCU itself. I'm using NUCLEO-H723ZG doing this which has DAC, COMP and TIM built-in.I've used 2 DAC for generate 2 simultaneous UART signals (If there's other ways to do this please recommend) but it's...

AMagk.1 by Associate II
  • 1103 Views
  • 0 replies
  • 0 kudos

How to send another START bit during an I2C transmission

Hi,I am trying to set the FRAM memory mb85rc64ta in sleep mode (Datasheet: I cannot copy and paste a link, but it is from Fujitsu and the pdf file is called MB85RC64TA-DS501-00044-4v1-E page 11)It requires 2 START condition but no STOP condition befo...

P M by Associate III
  • 8096 Views
  • 10 replies
  • 0 kudos

how can we send binary data on two different pins simultaneously on both the rising edge and falling edge of dclk whose speed can be 1MHz on stm32f4?

PCA is managed by a full-duplex serial interface. A typical data frame is defined bya burst of 8 DCLK pulses followed by an assertion of a DLOAD pulse (these lines are driven by the host printing system.). During each frame, 32 bits of control or pri...

SAMIN.1 by Associate III
  • 7283 Views
  • 14 replies
  • 0 kudos

STM32 Custom OTA Dual Bank Config

Hello There,I'm working on OTA application and successfully executed single bank OTA.Now I'm looking to switch to Dual bank operation to make it more reliable. So, there are 2 banks (memory areas) and after each update, the active bank changes. Means...

KAgga.1 by Associate III
  • 967 Views
  • 0 replies
  • 0 kudos