STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

single DMA buffer for two timers STM32G0xx

Hello. In a project with stm32g030 (071) I use two different timers to generate two PWM signals. The triggering of timers and PWM signals is out of phase by 180 degrees. Can I use one DMA buffer to load data into CCMR registers of two different timer...

Akoli.2 by Associate III
  • 1507 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H735V (LQFP100) PC2_C and PC3_C speed

Hello,I have a problem with pins PC2_C and PC3_C on STM32H7. We have custom board based on this MCU and we want to interface SD card via SPI. We are using these pins: PA9 as SCK, PA0 as CS, PC2_C and PC3_C as MISO and MOSI respectively. I can not ini...

0693W00000BdYQyQAN.png 0693W00000BdYBUQA3.png
heveskar by Senior
  • 10709 Views
  • 14 replies
  • 1 kudos

lsm6ds3 registers problem

Hi everyone!I'm using a custom board with an stm32l051 and an lsm6ds3(and two 4.7kohm pull-ups). I am setuping the I2C1 (pins PB7 SDA and PB8 SCL). then I do the IMU setup in which I write some values to control registers on the IMU. then I read the ...

0693W00000Nse3ZQAR.png
EPora.1 by Associate II
  • 1867 Views
  • 3 replies
  • 0 kudos