User Activity

I'm trying to use fileX for format a card with filex with exfat but having some issues, after the format when I create a file the file says it is already created, presumably from a previous format, possibly with regular FAT.Currently calling as stat...
Hi, I am experimenting with sending data across queues and noticed that if the queue size is just one deep I would expect a second attempt to add to the queue to wait until the corresponding receive function is called.However after a first call to tx...
HiIn the various filex with SDMMC examples the icache and dcache are enabled so when porting I did the same.I noticed when attempting to use DMA SPI it was not working until I disabled these. For the SD I then have to disable cache and cache manageme...
Hi, I am using STM32H725 with the FMC interface and trying to clarify some issues.The initial issue was seeing extra writes/reads on the bus - this seemed to be fixed by switching the banks to use the 0xC...0 address range or configuring the original...
Hi, we are using an STM32G05 series processor (STM32G051K6T6).The default setting in the Cube Programmer software sets the option byte nBOOT_SEL to high. This effectively disables the BOOT0 pin and prevents reprogramming if the option byte was not cl...
Kudos from