cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I have a short circuit between the RESET and the VCC. I measure a impedance of 1ohm between these two signals and 80ohm with the GND. The RESET pin only goes on a 0.1UF capacitor and on the programming connector.

ludovic-micou2
Associate III

the ST-LINK can't detect the micro but the software who is already programmed in the micro work perfectly.

Does anyone have an explanation why the reset breaks like this?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

If NRST is shorted to VCC, there's a hardware error or you've damaged the chip. There's no setting you can enable that would do this.

Likewise, if VCC has 80 Ohm impedance to ground, that also indicates a likely hardware error.

Also possible you're measuring it incorrectly, such as with the debugger attached or with it powered.

If you feel a post has answered your question, please click "Accept as Solution".
lmico.1
Associate

The measurement was made with the power and probe cables disconnected from the board. The measurement