STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f469 SDRAM Read/Write issue on FMC Bank2

Hello all,I have W9816G6JH( Winbond) SDRAM interfaced with STM32f469 on a custom board.SDRAM is interfaced on FMC Bank2.I have generated SDRAM initialization code for MDK-ARM using CubeMx. When I Write and Read back on SDRAM address 0xD0000000 it sho...

JShin.4 by Associate
  • 1278 Views
  • 0 replies
  • 0 kudos

STM32F407 - Question of how to use 3-wire SPI

Hi,My slave device has only one bidirectional data line. Now I want to configure the SPI in the half-duplex mode. And I noticed that the reference manual gave an descripiton of 1 clock and 1 bidirectional data wire.I want to ask if ST has peripheral ...

0693W00000QMnKhQAL.png
JGu.2 by Associate
  • 2495 Views
  • 2 replies
  • 0 kudos

SPI stops working when enable I2C?

Hello, I'm trying to use I2C and SPI simultaneously on an STM32F103C6TX.Both are working properly when only one of them is activated. However, when activating I2C peripheral with SPI already activated, SPI clock still works but the MOSI pin stops wor...

MCris.4 by Associate II
  • 3639 Views
  • 5 replies
  • 0 kudos

STM32 memory out and how avoid that

Hi there,here i'm for ask another help. I compile my program with keil and i read this data :Program Size: Code=15988 RO-data=360 RW-data=24 ZI-data=2088  How i can interpret ? I use one STM32G031F4P6 wher i have 8K of RAM and 16K of program. So i ju...

SGian.1 by Senior
  • 6520 Views
  • 11 replies
  • 0 kudos

Which STM32 controller has secure booting capability?

Im currently building boot loader to securely boot the firmware by signing the firmware images and verification during the boot of the firmware.So i'm using controllers like stm32f411,stm32f446,stm32f746 and stm32h723 ,I believe from the available do...

Yashwanth by Associate II
  • 2881 Views
  • 2 replies
  • 0 kudos

Timmer input STM32F429

Fig 9 of the STM32F429 datasheet it effectively states that the external source clock/signal has to be 1/3 of the Timer clock – makes sense as you want to ensure you capture the edge of the input signal. However, the Ref manual section 17.4.3, the re...

Reading Encoder pulses using external interrupts

I'm using STM32L451VCI6 MCU to read pulses from a rotary encoder attached to the shaft of a stepper motor using external interrupts. I'm incrementing a counter at rising edge of interrupt.According to spec of the encoder, I should be able to read 400...

NSure.1 by Associate
  • 2802 Views
  • 3 replies
  • 0 kudos