cancel
Showing results for 
Search instead for 
Did you mean: 

CAN TX stopped working

SPati.9
Associate II

Hello, I'm using stm32F446RE.

Sending CAN messages to two controllers and it stopped working after some seconds if time delay between the messages is less than one second, And it's slow for my project.

looking for suggestions, attaching some of my code:

txHeader.DLC = 4;

 txHeader.IDE = CAN_ID_EXT;

 txHeader.RTR = CAN_RTR_DATA;

 txHeader.TransmitGlobalTime = ENABLE;

       HAL_CAN_Start(&hcan1); //Initialize CAN Bus

       HAL_CAN_ActivateNotification(&hcan1,CAN_IT_RX_FIFO0_MSG_PENDING);

in loop:

txHeader.ExtId = 0x06D;

if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, stmp, &canMailbox) != HAL_OK) {Error_Handler (); }

HAL_Delay(100);

txHeader.ExtId = 0x057;

if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, stmp, &canMailbox) != HAL_OK){Error_Handler ();}

HAL_Delay (100);

Clock is HSE,@ 84Hz

             

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0