cancel
Showing results for 
Search instead for 
Did you mean: 

May I ask what is the silk screen of the material STM32F301K8U7, we are coming from F3018K7, but the specification is F3018K, which one is correct?

EJian.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @EJian.1​, to the community!

The STM32F301K8U7 has the marking F301K87 (not F3018K7).

The marking F301K8 (not F3018K) stands for the STM32F301K8U6, i.e. the temperature range of -40...+85°C instead of -40...-105°C.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.