STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Fluctuation

Hello,I have a ADC clock running at 96MHz prescaler divided by 10, 12bit, Sampling time 47.5 Cycles. I am just trying to sample this DC volgtages.  I have a battery that has around 20Volts, and I am stepping this voltage down using the voltage divide...

ytshin0877_4-1758084688725.png ytshin0877_0-1758083861526.png ytshin0877_3-1758084135450.png

Resolved! STM32H725VGH6 / Direct SMPS Supply / VLXSMPS Connection

Hi,We are using the STM32H725VGH6 MCU and are plannign to use the internal SMPS for VCORE.With regards to the connections required for the VLXSMPS pin, I would just like to confirm that a 220pF capacitor is required on this pin in the "Direct SMPS Su...

Figure3.png Table2.png Figure2.png
SammExa by Associate
  • 5100 Views
  • 5 replies
  • 2 kudos

STM32G030C8T6 readout protection doesn't work

I tried to set readout protection via ST-LINK CLI - it's enabled and disabled correctly, but after RDP=0 I can't erase/write chip - I've got an error on write operation. Tested on 2 boards and both boards have same behavior. e:\STM32 projects>"%PROGR...

NiTr0man by Associate III
  • 980 Views
  • 5 replies
  • 2 kudos

Resolved! STM32H747-DISCO Core-Lock Problem

Hello,I’m using the STM32H747. When I set the RCC power source to RCC → Power parameters → Supply source = LDO, the core locks up; if I select SMPS, there’s no issue.When I set CM7 to its maximum clock frequency (480 MHz) and CM4 to 240 MHz, the tool...

CKILI.2 by Associate II
  • 1642 Views
  • 3 replies
  • 0 kudos

STM32L562 UART Data Rx packet loss

Hi,I am using USART4 in STM32L562E-DK eval board. with given configuration. In which I am able to transmit the data correctly on TX based on which UART slave device is sending back the 4 bytes ACK and 16 bytes RESPONSE.Using following codevoid HAL_UA...

414D414E_0-1757398146959.png
414D414E by Associate
  • 1089 Views
  • 5 replies
  • 2 kudos

i2s clock issue in stm32h723zg

hello, i hope you are doing good. i am facing an issue in configuring i2s in dev board nucleo-h723zissue i am facing is no clock at i2s2-sck pin.i tries all other i2s port also. i checked clock through logic analyzer .here is my clock configuration: ...

sajidehsan194_0-1757422544161.png sajidehsan194_1-1757422574730.png sajidehsan194_2-1757422636993.png

Resolved! STM32H743VIT6 ADC didn't run

Dear all!i'm handle graduation thesis project: " design driver for PMSM using STM32 base external mode with Matlab simulink"i design hardware as PDF file, all block working without ADC, i try to set up by STM32cubeMX 6.14 but it still can't run, so c...

Bootloader for STM32F746 for firmware and QSPI

Apparently I can not easily update my application firmware for stm32F746 toughGFX app with just one Bin file. I have written a bootloader for an SD card. It loads firmware at 0x08040000. I am not sure I understand everything that is going on here, so...

FJB2069 by Senior
  • 545 Views
  • 1 replies
  • 0 kudos