cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5xx 100 pin - which one for MIPI DSI and which one for parallel RGB LCD

logstream76
Associate II

Hi,

In my next project I would like to use 2 type of displays. One with MIPI DSI interface and the other with parallel RGB.
That is why I chose microcontrollers from the STM32U5 series ( vector graphics accelelator ).
According to the information on the ST website, the series (100 pin):
STM32U5G7VJ and U5F7VJ support RGB interface and STM32U5G9VJ and U5F9VJ support MIPI DSI

However, inside the datasheet of the series: STM32U5F7xx in the section describing the pin layout there are 2 types of 100 pin packages:
"LQFP100 SMPS" - there is no MIPI DSI pins
"LQFP100 DSI SMPS" - has pins to support MIPI DSI (7,8,10,11)

And now I am completely confused.
The question is which STM32U5xxxx (100pin) chip should I order to support RGB and which one to support MIPI DSI ??

Tomasz

1 ACCEPTED SOLUTION

Accepted Solutions

Dear @logstream76 ,

Thank you , we will check it ! A bit complex to handle common Libraries & symbols for different parts . 

Ciao 

STOne-22

View solution in original post

3 REPLIES 3
STOne-32
ST Employee

Dear @logstream76 ,

 

You can check at end of the datasheets the Ordering information.   MIPI DSI is only available for STM32U5G/F9 version not for STM32U5G/F7 version

 

STOne32_0-1743250294980.png

STOne32_1-1743250535756.png

 

Hope it helps you.

STOne-32.

Thank you.

The schematic symbol shown in your e-store is misleading.
It shows that U5F7 also has DSI pins:

STM32U5F7VJT6Q_store.jpg

Dear @logstream76 ,

Thank you , we will check it ! A bit complex to handle common Libraries & symbols for different parts . 

Ciao 

STOne-22