User Activity

Hello,I have a NUCLEO-F446RE board, lots of homemade boards with little MCUs (STM32G030F6, STM32F103C6, ...), some blue pills and programmers. Only the first ones I bought has an original chip. The other blue pills and programmers, the vendor lies an...
Hello,When I plug this board to my computer, appears a removable disk of 1,6 MB capacity.Is this disk accessible from the MCU? For store small data, or make a dataloggerWhere the filesystem is stored? Neither the STM32F446RE nor STM32F103CB of the ST...
Hello,I will make some probes for reading electrical values (AC, Analog, digital,...), but I'm not sure what happens if I insert a signal to a GPIO when MCU is powered off.I read time ago that all GPIOs are in high impedance state when MCU is not pow...
Hello,I made a project using a blue pill. It works when is powered through st-link (3,3V).When I power this board from two AA batteries (~3V), the board does nothing until I press the reset button.An STM32F103 should work from 2 to 3,6 V, according t...
Kudos from
Kudos given to