STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How is CAN message RAM initialized/zeroed on STM32H7?

I have the problem that the CAN message RAM which is allocated for the acceptance filters is not zeroed out on startup.The part of the CAN message RAM allocated for acceptance filter seems to just be random data which means that usually no CAN frames...

julianoes by Associate II
  • 1458 Views
  • 0 replies
  • 1 kudos

Trying to do an encoder with an FSM

Hello, right now im trying to do an encoder as a project for my digital electronics class. I've done it in two different ways, by functions and by switch cases, and neither seem to work. I have to make it so every time a switch of states ocurr within...

OMart.6 by Associate
  • 1625 Views
  • 2 replies
  • 0 kudos

When does FLASH lose data

在我的使用中,一些�?�数是在�?�片机(STM32F446ZET6)的闪存中�?置的,但在未知情况下�?�数丢失。在断电之�?,有断电和通电�?作。请问这是什么原因造�?的?解决方案是什么?

qli.3 by Associate
  • 1562 Views
  • 2 replies
  • 0 kudos

How to know what cause Error_Handler?

Often trip to Error_Handler from usb_device.c and usbd_conf.c.void Error_Handler(void){ /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CO...

STM32F429 to STM32H7A3 migration

Hello There,I'm looking to migrate from STM32F429ZIT6 to STM32H7A3ZIT6 for a TFT application.I have checked H7 will provide better performance on this.There is one more thing that comes to my mind that H7A3 has better specs than F429. Then why F429 p...

KAgga.1 by Associate III
  • 917 Views
  • 1 replies
  • 0 kudos

Resolved! Nucleo-U575zi-Q ADC reading garbage values

I'm new to the stm32MCU. I am using a Nucleo-U575zi-Q board. I am trying to read ADC values by setting the built-in DAC. I have check my DAC out and it is working fine. My ADC reading is giving me garbage values. I have set HAL_PWREx_EnableVddA() als...

ABhat.12 by Associate II
  • 2348 Views
  • 7 replies
  • 0 kudos

Debug problem

Hi, I have a problem where I cannot debug my code bcs of this error. Anyone know how to solve these problem?btw im using the STM32H750VBT6x for MCU and ST-LINK V2

0693W00000WJ9R2QAL.png
Angle by Associate II
  • 2372 Views
  • 8 replies
  • 0 kudos