STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Basic GPIO_init() question

I am using for instance, ADC, UARTS, Timers, external interrupts, etc., all generated with cube. But I notice that cube doesn't always generate GPIO settings for certain pins. For instance, ADC1_IN4, when I select it using my board, an stm32f769i-d...

ADC Converter in STM32H745

I use the STM32H745 under the CubeIDE. I thought, when I configure my ADC to trigger the interrupt from a timer, the HAL_ADC_ConvCpltCallback() function will becalled automatically. The related ISR is called and I can read out the value. But the Call...

JPiet.3 by Associate III
  • 1885 Views
  • 4 replies
  • 0 kudos

DMA Mem to peripheral inconsistent output

I have a timer + dma which outputs a signal for addressable LEDS. The code calls the PWM Start function on a crude timer loop for testing purposes.The first time the DMS starts, its perfect, and the output is correct and as expected. However the seco...

0693W00000SuEDcQAN.png 0693W00000SuEDwQAN.png

Resolved! stm32g431 boot 0 pb8

how disable boot 0 pin8 i used this pin for input make problem to boot from flash how can disable any condition mcu boot from flash not check this pin when reset