STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1KBT6 flash module organization

Hi good day, could you guys please tell me where i can get the STM32G0B1KBT6 flash module organization Table? i've looked for it on datasheet but found nothing

fasyr.1 by Associate II
  • 2568 Views
  • 4 replies
  • 2 kudos

How to reduce the time between SPI (DMA) transactions

I need to transfer a large amount of bits over SPI de-asserting/asserting the select line very 64 bits. I'm using DMA. The time between transmissions is huge, as can be seen below:The pink channel is SCK, each chunk is 64 bits. The code is below:whil...

0693W00000aHFGqQAO.png
DGast.1 by Associate III
  • 2899 Views
  • 3 replies
  • 0 kudos

Recovering from a failed I2C transfer

I am using HAL_I2C_Master_Transmit(). That generally works well. However, I sometimes run into an issue when the slave device is not responding. HAL_I2C_MasterTransmit() obviously returns an error after running into timeout, as it should. But then I ...

Is it possible to use the SAI peripheral with the data line only - SD_A or SD_B (without outputting the peripheral clock signal) when using the "free protocol" mode for a single-wire communication purposes?

Dear STM32 MCUs community,I am currently working on a project with the STM32l452RET6 MCU with a goal to use the SAI peripheral for one-directional single wire communication purposes, so only the "data line" (SD_A or SD_B) will be outputted using the ...

STM32F446 MCU LSE Ready Issue

Hello, I used STM32F446 MCU. I'm disconnecting the external RTC crystal. Then I turn the device off and on, but the LSERDY bit does not become zero. What could be the reason for this? Thanks.

Konkalat by Associate
  • 1452 Views
  • 1 replies
  • 0 kudos

Resolved! Weird ADC failure STM32F091, any ideas

We've been building a PCB with four STM32F091s on each PCB and we've built about 50 units by now (over about 3 years). I have now seen three PCBs where the ADC readings are 'bad' on two of the four micros. By 'bad' I mean conversion values are 30% is...