cancel
Showing results for 
Search instead for 
Did you mean: 

Receive parallel data in Nucleo_H743ZI2

AElta.1
Associate II

Hi

I am following the AN4666 document to receive parallel gpio data, with on clock input.

this is the code I wrote : I was expecting to receive gpio data and save to memory by triggering the DMA at every rising edge my issue is that the timer (input capture mode ) only detects the first rising once and save GPIO value in the first array once and then stops making whats left of my buffer equal to 0.

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32h7xx_ll_tim.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define BUFFER_SIZE 100
static uint8_t aDST_Buffer[BUFFER_SIZE] = {0};
int main(void)
{
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
  /* Configure the system clock */
  SystemClock_Config();
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART3_UART_Init();
  MX_USB_OTG_FS_PCD_Init();
  MX_TIM1_Init();
  MX_DMA_Init();
// Start DMA in interrupt mode, specify source and destination
  	HAL_DMA_Start_IT(htim1.hdma[TIM_DMA_ID_CC1], GPIOC_IDR, (uint32_t) &aDST_Buffer, 10);
// Enable timer to trigger DMA transfer - CC1DE bit
  	__HAL_TIM_ENABLE_DMA(&htim1, TIM_DMA_CC1);
// Enable timer to trigger DMA transfer - CC1DE bit
  	__HAL_TIM_ENABLE_DMA(&htim1, TIM_DMA_CC1);
while (1) {}
}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @AElta.1​ ,

Maybe it's related to this issue: DMA not working in CubeMX generated code - order of initialization

So, the MX_DMA_Init shall always be called before any other peripheral initialization, as mentioned in this post.

I hope this helps ! If this the case, please close this post by clicking the Select as Best button on my reply .

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello @AElta.1​ ,

Maybe it's related to this issue: DMA not working in CubeMX generated code - order of initialization

So, the MX_DMA_Init shall always be called before any other peripheral initialization, as mentioned in this post.

I hope this helps ! If this the case, please close this post by clicking the Select as Best button on my reply .

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen