STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! program hang up at "print..string" , same working on other positions and also was working before - have no idea anymore

breakpoint reached normal;from here this jumps to "show.."and then this breakpoint seems never reached, but when going step by stepline 1354 is reached and also the following "sprintf.." , but it gets curious:when "Radio.." text is selected , is draw...

0693W00000aHd6uQAC.png 0693W00000aHd4wQAC.png 0693W00000aHdFmQAK.png
AScha.3 by Super User
  • 2326 Views
  • 7 replies
  • 0 kudos

Resolved! HAL I2S Receive DMA mode stuck in BUSY mode

On a stm32 mcu, using HAL_I2S_Receive_DMA the clock generation is started. At first, the application went into a hard fault and nothing is subsequently written in the data receive buffer.HardFault_Handler:08000942:  push  {r7}08000944:  add   r7, sp,...

jess by Associate II
  • 2521 Views
  • 2 replies
  • 0 kudos

MCP2515 Module Library

Hello,I would like to use MCP2515 module which can be found here. Is there any tested official or nonoffical library that I can use with stm32f429-disco developer kit? Thanks inadvanced.

Öyild.1 by Associate II
  • 9725 Views
  • 7 replies
  • 0 kudos

writing single byte in flash

I'm trying to write on the flash of the stm32u5 microcontroller. Why in the flash driver, in particular in the file stm32u5xx_hal_flash.c, is present only FLASH_TYPEPROGRAM_QUADWORD and FLASH_TYPEPROGRAM_BURST? Is it not possible to write on the flas...

IVent.1 by Senior
  • 1636 Views
  • 2 replies
  • 0 kudos

HAL_UART_RxCpltCallback() doesn't trigger

I am working on a STL32F401RET6 MCU and the HAL_UART_RxCpltCallback() doesn't work even though I turned the global interrupt on.Here is my code for the callback functions : void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { HAL_GPIO_T...

LBiss.1 by Associate
  • 7389 Views
  • 3 replies
  • 0 kudos

CANbus: Check if CAN message failed to send X number of times

Hello,I am working on a CANbus communication with a critical system component that, if it is NOT communicating, portions of the systems should be shut down. I am trying to come up with a way to determine if communication is lost, but I feel like the ...

KMew by Senior III
  • 1016 Views
  • 0 replies
  • 0 kudos

STM32G0B1RE FDCAN normal / external loopback issue

Hi everyone,I am currently experiencing some issues with the FDCAN interface; my setup consists of two nucleo boards (Nucleo-G0B1RE) which use FDCAN interface to communicate with each other. As transceivers I am using two ATA6563-click boards.The clo...

0693W00000aHcAbQAK.png 0693W00000aHcAqQAK.png 0693W00000aHcC3QAK.jpg 0693W00000aHcAmQAK.jpg
lr2 by Associate
  • 1940 Views
  • 0 replies
  • 1 kudos

Resolved! Cannot get OCTOSPI example for STM32U575ZI MCU to work

Hello everyone,I am currently trying to connect a APS51208N PSRAM to a STM32U575ZIT6 using the OCTOSPI interface. I followed the steps for the first example in application note AN5050 (chapter 5.2.5, number 1). However when I step through the program...

PKolo.1 by Associate II
  • 3496 Views
  • 2 replies
  • 0 kudos