STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In STM32L562VET6Q Microcontroller in that my question is how to configure/map SRAM 2 memory address as 0x2003 0000, so , i can use it as contiguous memory of both SRAM 1 and SRAM 2 i need big size continuous memory block.

"64 Kbytes located at address 0x0A03 0000 with hardware parity check (SRAM2). This memory is also mapped at address 0x2003 0000 offering a contiguous address space with the SRAM1"

sra by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

STM32G0B1 Device lock?

Hi, I am currently trying to develop a DFU using the chip's dual bank feature.After bricking my second prototype (only recoverable by exchanging the G0) I am out of ideas what could be the problem.I could at least track it down to manipulation of the...

Schue by Associate II
  • 1875 Views
  • 2 replies
  • 0 kudos

Wordlength setting when using Modbus RTU as UART

Hello, Now I'm using Modbus RTU and UART. Modbus RTU communication is being performed through UART. Modbus RTU setting is data 8 bytes, but communication is possible only when uart wordlength is set to 9 in STMcubeIDE. Why is wordlength 9 when data i...

dkim.3 by Associate II
  • 2259 Views
  • 2 replies
  • 0 kudos