STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F334 TrueStudio - Adding libarm_cortexM4lf_math.a Getting error: arm-atollic-eabi/bin/ld.exe: <WWDG_EXAMPLE>.elf section `.rodata' will not fit in region `FLASH' and region `FLASH' overflowed by 101180 byte

The size looks like around 107KB of libarm_cortexM4lf_math.a library, the total flash is 64KB in STM32F334x SoC. Could you let me know if I want to perform FFT (Fast Fourier Transformation), is there any alternative or light weight library I can use....

MAlam.6 by Associate II
  • 1317 Views
  • 1 replies
  • 0 kudos

Resolved! Error in Datasheet DS12712 Rev 4

Hello,i found an error in the Datasheet DS12712 Rev 4 of the STM32G473 Controller.Can someone clarify please what will be correct:In Chapter 4.11 - "Alternate functions" it tells, that PA10 has an alternate funktion AF2 for I2C3_SCLBut in Chapter 4.1...

Moritz1 by Associate III
  • 1262 Views
  • 2 replies
  • 0 kudos

Initialize SDRAM in SystemInit

Hello,I am using a STM32H7A3 and a SDRAM MT48LC8M16A2P.In a project using the emWin graphic library, I would want to store the relative buffer 'aMemory' in SDRAM.By reading on community and seeing the examples I understood that I have to write a Syst...

Cannot post comment in my case

I have a case open in my profile due to technical issue with one disco board and the ST employees are updating me on the situation. I would like to reply to them but I keep getting an error whenever I try to post a comment.See screenshot for referenc...

0693W00000aJKtwQAG.png

Trying to use PWM to toggle LED, won't output to LED

Hi folks​New to STM32 and getting into it by starting with clocks, timers and ADC. All I want to do is dim a few of the onboard LED's with a pot on a breadboard. Stepping through debug I've found the following Analog input is reading values from the ...

SG.121 by Associate II
  • 5417 Views
  • 8 replies
  • 0 kudos