STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

removing chip cause unexplainable artifact.

I have a st chip (HT35) with the STM32H735G-DK Discovery Kit. Projects was complete and running fine. We then had to remove the OCTO SPI nor flash chip because we need access to Pe2. but after removing the chip the app froze after MX_TIM4_Init(). The...

ulao by Associate III
  • 3585 Views
  • 9 replies
  • 0 kudos

Multi-channel ADC reading in continuous mode.

Using an STM32H757-EVAL (don't use CM4) with CubeMX. Configured my ADC1 as follows:DMA is:Start the process as follows (both calls return HAL_OK):I allow the code to run for 10 seconds and break. The m_hv_status_values buffer still has the initial va...

_legacyfs_online_stmicro_images_0693W00000bjjM0QAI.png _legacyfs_online_stmicro_images_0693W00000bjjMAQAY.png _legacyfs_online_stmicro_images_0693W00000bjjMFQAY.png
Gil1 by Associate III
  • 3817 Views
  • 2 replies
  • 0 kudos

skip flash erase before programming

hello,Which command is valid to do this? I see --skipErase, I have also seen --ske, or ske as possible commands to use. What is the syntax for this command? I dont see a reference in the manual...Please help thanks in advance.

RobNeWin by Associate II
  • 1723 Views
  • 2 replies
  • 0 kudos

STM32L4 - SMBus and Melexis MLX90614

Posted on May 23, 2018 at 17:49Hello,I'm trying to read temperature values from a Melexis MLX90614 sensor with SMBus but something seems to be wrong.I used the HAL_SMBUS_IsDeviceReady to see if I can connect to the sensor and I can.#define MLX90614_...