STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to integrate SPI sd card on STM32L452CC?

I have a custom board with the l452cc controller. I am trying to run an sd card with fatfs through spi. I have generated cubemx fatfs files, but there is no interface layer for spi to fatfs. Are there some examples I can reference off of, or what is ...

MFrie.6 by Associate III
  • 10712 Views
  • 19 replies
  • 0 kudos

STM32F407 Discovery board and TLC5947

Hi I'm new to using STM Microcontrollers and I have the Discovery board as my development board, I have used Arduino religiously and thought I should learn something new.I have learnt how to modify data registers, for example, turn the 4 LEDs on and ...

VYada.3 by Associate II
  • 4376 Views
  • 8 replies
  • 0 kudos

Having a difficult time using SPI SD-card with STM32F446

I am having a very difficult time trying to read the file directory using the code I got from the web. I am able to get most SD card functions to work and I actually get the read directory function to work the first time but it only reads 6 of the 1...

CBarb.1 by Associate III
  • 1076 Views
  • 0 replies
  • 0 kudos

How many mhz oscillator can run or external clock mod 2 ?

I am using STM32F030C8T6TR. I have a process that needs to be counted precisely, so I'm connecting a timer oven oscillator with an extenal clock mod 2. How many MHz can I use( for maximum)? I'm using an internal clock for processor, it works at maxi...

hdemi.1 by Associate III
  • 2184 Views
  • 3 replies
  • 0 kudos

Resolved! Why SMT32L031x UART pins do not work?

Hello, I have a custom board with a SMT32L031F6P6 on it: PA2 and PA3 USART2 channel seems not to work even if they are correctly set in the .ioc file.I have tried the same code on the NUCLEO-L031K6 board using VCP-TX and VCP-RX (PA2 e PA15) default p...

LSant.7 by Associate II
  • 1952 Views
  • 3 replies
  • 0 kudos