User Activity

I generated a touchgfx project and figured out the structures. I am able to change the chart and plot new data. What I don't understand is the generator it allows me to create multiple lines but I can't figure out a way two separate the data or add...
I've been working with the cubeide and touchGFX. It seemed to be working but when I tried to import another project, the IDE gave me a message stating that, even though the new TGFX project was named something else, it was going to import it as the ...
I searched and saw others had this problem but for the life of me, I can't figure out how to see the answers to the questions when I search? I hit every button and arrow but nothing show the answers.Setting that aside, I need to include .hpp files i...
My application has a low priority usart receive function - meaning that if characters are delayed it's no big deal. I've been using interrupts with a callback receiving one character at at time with a read always outstanding. I process flags and b...
I can make an application and load it into the IDE. I'm very familiar with programming the STM32s. I created a simple app that creates a dynamic chart. I can see where the dummy data is loaded into the chart in the base code. I have a few questions ...
Kudos from