STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PC13 disturbs LSE erratum is widespread

Trying to answer https://community.st.com/s/question/0D53W00002HBKtaSAH/stm32l452-lse-pc13-errata I realized it's a widespread erratum which recently appeared in most older STM32 errata.I understand that issues like these may surface after years. OTO...

Resolved! Repeated Start bit code without memory address

I am using a Flintec TR2 board, and I want to communicate with it via my STM32 L496zg Nucleo Board. It uses I2C repeated start condition to communicate. Most of the codes I found online suggest using HAL_I2C_Mem_Read/Write functions but the user manu...

AVima.1 by Associate
  • 1518 Views
  • 2 replies
  • 0 kudos

STM32F745 - Disable Watchdog in Sleep mode

Hello,I am using STM32F745VEHx. I would like to disable the software independent watchdog before microcontroller goes into Sleep low power mode and then re-enable it once microcontroller comes out of Sleep. I can find literature which suggests this c...

LJain.1 by Associate II
  • 1330 Views
  • 1 replies
  • 0 kudos

STM32F303K8 - Sampling a 40KHz sine-wave

The problemI am to compare the phase shift between two sinewaves from an external source (I used a function generator in this case). I am running the STM32F303K8 at 64MHz, and this clock goes directly to the ADC and Timers 1 and 2 as well with a pres...

_legacyfs_online_stmicro_images_0693W00000bku8LQAQ.png _legacyfs_online_stmicro_images_0693W00000bku8kQAA.png
malehakim by Associate III
  • 4298 Views
  • 3 replies
  • 0 kudos

Resolved! stm32f334 i2c slave speed

Stm32f334 i2c works in slave mode , select i2c kernel clock 72mhz. datasheet says it's i2c fast-mode+ support up to 1mhz, but I found that it can be accessed stably by a master with scl at 2.5mhz. Is it ok to use a master scl speed faster than...

tri.1 by Associate
  • 2380 Views
  • 1 replies
  • 0 kudos

STM32F429 SD card rcvr_datablock time

I have a application with STM32F429ZI and SD card withour RTOS.I have a llong time for write in a SD card.The rcvr_datablock routine is loong about 3 ms between set and reset LED !!!It is possible to reduce this time using rot_rdq without use a RTOS ...

IlConte by Associate III
  • 868 Views
  • 0 replies
  • 0 kudos

Resolved! TM32H573xx + TrustZone activated

Hi guys! I am a newbie in the STM32 world. I am little bit curious about STM32H573xx series's TrustZone feature implementation. My question is: if I develop a firmware by enabling the TrustZone (TZEN=1) and then every time when I will write the file ...

GTest.1 by Associate II
  • 1914 Views
  • 2 replies
  • 0 kudos