User Activity

I want to monitor battery voltage (Vbat). I use the adc function to monitor voltage on the Vbat pin, and it can't read the voltage. When I use the same function on other pins, it can read correctly. For Vbat monitoring, what are the specific configur...
Hello, I need some help. I have problem about CAN bus. I connect the wire to the header pin. It swaps between CANH and CANL. Can STM32 force CAN_TX pin to CAN_RX pin and CAN_RX pin to CAN_TX pin? If not, do you have another solution?In my case, I can...
I want to read and write data from Flash via spi. I try some tutorial, He tell me to config and use some library.I do it but it don't work. MCU:STM32L496ZGT6Flash: S25FL128LAGMFB010
I'm looking for chip for my project. I don't understand about code of STM32L496ZGTx, what is the difference.