STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connection of Power and XSPI

Hi,This is my first time using an STM32N6 without internal flash, and since I am right before handing over files for artwork, I would appreciate it if you could check if the power lines and XSPI memory connections are correct.I have searched around a...

pic1.png pic2.png

Resolved! Problem to set FDCAN2 in STM32CubeMX for STM32H562RGT6

Hello,I am planning to use STM32H562RGT6 in my product to communicate and update my firmware via CAN FD.To plan that, I am using STM32CubeMX 6.17.0, the datasheet and the AN2606 (Rev 70).And I would like to use only one CAN FD to communicate and to u...

x314159_1-1776260323976.png x314159_2-1776260360172.png x314159_3-1776260415863.png
x314159 by Associate
  • 218 Views
  • 3 replies
  • 2 kudos

Resolved! Wrong voltage typed at Vrefint STM32C092

I have followed the datasheets and tried to calculate my reference voltage. I am supplying steady 3V on Vref+ pin but I wanted to confirm this because I have some troubles with the ADC precision.So I read the internal voltage both on my card and on a...

morris_0-1776092976724.png Skärmbild 2026-04-13 153204.png
morris by Associate III
  • 198 Views
  • 3 replies
  • 1 kudos

Need help in erasing the device: STM32H735IGK3

HiI need help in erasing the device: STM32H735IGK3, This device is getting erased only till sector 0.There were total 8 sectors.I am following the steps given in  Reference manual for erase operation but still it didn't work.Could you please suggest ...

Saista by Associate
  • 135 Views
  • 2 replies
  • 0 kudos

Issue Interfacing with AP memory.

Greetingwhat want to achiveThe current state.What we have tried.Hey there Community,We are running a project were we need to interface with an AP memory on a custom made board. We intend on using the PSRAM for image capture for a 5mpx image dumped by...