cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 unused XSPI pins

batuhanky
Associate III

Hi all,

I'm designing STM32N655L0 based board and I've one question.

I'm using XSPI1 and XSPI 2 peripherals.

  • XSPI2->Octa SPI mode, NOR Flash
  • XSPI1-> SDRAM, Hexa SPI

So my question is can I use unused CS, NCLK pins as an IO?

I just wanted to be sure.

 

BR

1 ACCEPTED SOLUTION

Accepted Solutions
ELABI.1
ST Employee

Hi @batuhanky 

Yes, it's possible. Just be sure that these GPIOs are not used and not interfaced with external memories.

Thank you.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
ELABI.1
ST Employee

Hi @batuhanky 

Yes, it's possible. Just be sure that these GPIOs are not used and not interfaced with external memories.

Thank you.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.