STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Fluctuations in ADC value of STM32H743 MCU

Hi,I have been working with STM ADC’s from quite a long time. I had used STM32F373 and F4 series MCU ADC’s earlier for my applications. As, now my application requires huge amount of RAM, memory and computation speed I have shifted to STM32H743 MCU ....

James1 by Associate II
  • 23233 Views
  • 26 replies
  • 3 kudos

DMA - from SPI to DAC - 16 bit

Hi,I use DMA for transfer data from external flash memory to DAC for playing sounds - in 8 bits mode like that:1) TIM6  gives impulses to DMA_1 - which transmit  dummy byte to external flash in 8 khz intervals (Fsampling of sound). External flash alw...

JR2963 by Senior II
  • 1865 Views
  • 2 replies
  • 0 kudos

Multiple pulses are generated on GPO pin for ST25DV64KC micro, when NFC enabled mobile is kept near the antenna, it is expected to have only two pulses for RF activity entry and RF activity exit conditions

Hi,I am using ST25DV64KC micro for NFC communication interfaced with SAML micro controller. I have kept the setting for GPO signal as I should two pulses for every RF read/write session, first one indicating RF field is active and another one indicat...

SSBH by Associate
  • 1191 Views
  • 1 replies
  • 0 kudos

STM32 development board for CAN/OBDII development

Hello. I am looking for STM32 based development board for CAN/OBDII development. Please suggest me some suitable supportive development board based on STM32F4 or H series which has inbuilt CAN support and if it has CAN/OBDII development support examp...

ASh.1 by Associate II
  • 4273 Views
  • 6 replies
  • 2 kudos

Resolved! Help with Led blinking - STM32F7508-DK

Hi folks, first off all I'd say to that I'm really new to MCU and for some silly reason I went for a STM32F7508-DK as my first board of STM3. With that being said, I'm asking for help on why my Led blinking code is not working,/* USER CODE BEGIN Head...

MCosm.3 by Associate
  • 3934 Views
  • 4 replies
  • 1 kudos

Best use of timer and timer modes

Hello all and tks for reading,I will develop a three-phase 60Hz rectifier, 12 pulses, thyristor controlled. The mpu to be used is the stm32f303RE and I will make the prototype on a Nucleo-64 board.The mpu control signals will go to an already existin...

LCatL by Associate II
  • 3076 Views
  • 2 replies
  • 0 kudos

I am using a STM32G474 and testing it in a nucleo-64 board. When I enable the hardware window watchdog and the hardware independent watchdog my software does not run. it seems to get stuck after each startUp.

The hardware watchdogs is set through an option byte modification done by software and right afterwards the WWDG and IWDG init functions are called as well as the refresh API, called periodically. If I change my code to use the SW WWDG and IWDG then ...

AMija.1 by Associate
  • 1431 Views
  • 1 replies
  • 1 kudos