STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Neucleo Dev Board Schematic

Is there a schematic or a reference design similar to the one used for the Neucleo boards?  I'm thinking of spinning up my own board instead of using a neucleo, and wanted to include design elements like the debug link, boot loader link, oscillators,...

LMorr.3 by Senior II
  • 2064 Views
  • 1 replies
  • 2 kudos

CANBUS Between two STM controllers

Hello I am trying to attempt a CANBUS communication between two different STM boards, I've been following the videos on the STM website as a reference and I got the LOOPBACK Mode to work with one STM board but I am having trouble getting the NORMAL m...

How make for Stm32F407G-DISC1 with Tim

I try make"design system that sets outputPin (should be digital gpio output ) high for 0.25 secs,and low for 0.25 secs."and i use  GPIOA_PIN4(input) and   GPIOB_PIN0(output), I'm new to stm32, I'm having trouble with the timer.I try use tim, how can ...

Pogomo_0-1687702071371.png
Pogomo by Associate
  • 3067 Views
  • 5 replies
  • 0 kudos

FLASH_Type_Program lists a word as 32 bits?

I'm writing a bootloader and trying to use HAL_FLASH_Program() and noticed that a word is listed as 32 bits.  Is this an ST specific word size?  I've always thought that a word = 2 bytes = 16 bits.  But it appears that if I want to write a word with ...

Resolved! Problem with UART transmission

Hi everyone,Do you think there is any reason why a set of instructions (20 lines max.), including UART transmission, works fine within the while(1) block but it doesn't work if that exact set of instruction is in a function, within the same while(1) ...

mdiro by Associate III
  • 2975 Views
  • 5 replies
  • 0 kudos

Can a Debugger Be Used to Program TCM RAM STM32H730

Hi, I am working on a project using the STM32H730. In order to accommodate a requirement for larger program memory size we are planning on using an external flash and loading instructions into TCM RAM on boot. My question is whether for development w...

EPala.2 by Senior
  • 2803 Views
  • 6 replies
  • 0 kudos

STM32H7 M7 stop mode issue

Hi,I have a bit of a problem.Currently I´m using the M7 to do all the work, it initializes all the peripherals it needs.The M4 waits for M7 to configure stuff and then goto standby mode.The problem is related to sleep/stop/standby mode of the differe...

AJans.3 by Associate II
  • 1319 Views
  • 0 replies
  • 0 kudos

PID controller

Hello ST Community,I am generating a PWM signal with sample frequency of 10KHz on STM32F4 nucleo board with a clock frequency of 82 MHz.At the same time, I am programming a PI controller; to make sure that my PI regulator works also with 10KHz freque...