User Activity

Dear Experts,I am a new user for Cube-monitor.I want to output data buffer graph on the cube-monitor screen.The data buffer unit size is 16 bits and total is 1024.(declaration will be "uint16_t buffer[1024];")Is this possible and if so, how do I do i...
Hello,I have question about gps speed prediction in the tunnel.When gps loses signal in the tunnel, we can not get any speed info from gps.In that case, can we predict speed using mems? If yes, how to solve that?Thanks in advance for your advice.Best...
Hello, I want to use Uart6 interrupt on STM32H750b DK board, but it doesn't work, so I'm asking here. Is there anyone used uart on stm32H7xx chip?I just added the Uart-code using CubeMX and then when I build/start debugging, it stopped during initial...
Dear CubeIDE team,I just started using CubeIDE.Following are my question.1. How can I find string text in .h file?    I tried to "ADC_OVR_DATA_OVERWRITTEN" string in Drivers\..\inc using "Ctrl+H" but I failed.    This is very uncomfortable to use. No...
Dear All,I have question about manipulating cubemonitor.I want to display 1024 buffer data to the graph on the cube-monitor at once.Is it possible?Thanks in advance for your advice.BR,TommyLim