STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to configure I3C port on NUCLEO-H503

Hello.I'm trying to make an I3C Master device using the NUCLEO-H503 board.I am trying to implement GPIO by directly controlling, without using HAL Library.However, I3C port uses both Open Drain and Push pull,Is it possible to implement this function ...

sh.lee by Associate II
  • 3095 Views
  • 2 replies
  • 2 kudos

WWDG RESET Due to osDelay

Behaviour of WWDG on STM32L071KZUx.We are trying to read and write 256bytes from the Slave. In a specific case the Slave needs delay of 120ms to process the data when we add 120ms of delay in the MCU, the void HAL_WWDG_EarlyWakeupCallback(WWDG_Handle...

VSoun.1 by Associate II
  • 4303 Views
  • 2 replies
  • 0 kudos

STM32U585 Smart Card Communication

Hi AllWe are testing the STM32U585 Smart Card mode with clock and trying to connect with external SAM module. We are able to get the USART-ISO7816 frame format from the controller but we are unable to capture the ATR value from the module in a correc...

PJose4_0-1687771024546.png PJose4_1-1687771062858.png
PJose.4 by Senior
  • 7040 Views
  • 13 replies
  • 0 kudos

Resolved! STM32F446 TIM2 CCR1 and DMAR registers appear tied together.

I've been trying to get TIM2 PWM (or even OC) to produce an output. When looking at the registers, using openocd w telnet, I find that setting 0x40000000 (the CR1 register) with 0x81 also sets the 0x4000004C (the DMAR) register. The reverse is the sa...

DHase.1 by Associate III
  • 1704 Views
  • 2 replies
  • 0 kudos

STM32F446 TIM2 16b versus 32b conflict in RM

I'm having trouble getting TIM2 PWM to work so I've been studying the RM closely. The following conflict came to light.The RM shows TIMx_ARR and TIMx_CNT as 16b, but TIMx_CCR1,2,3,4 as 32b. The text (section 17.2) says TIM2 & TIM5 are 32b. Some debug...

DHase.1 by Associate III
  • 1306 Views
  • 1 replies
  • 0 kudos

External debugger NUCLEO-H743ZI2

The goal: Debug the NUCLEO-H743ZI2 with Tracealyzer.To do it I have to connect the board with my computer via jlink. I found the tool STLinkReflash, that can emulates the jlink in the stlink. The problem I found is that it does not work for the stlin...

Manu Gr by Associate
  • 2068 Views
  • 3 replies
  • 0 kudos

Resolved! Timer Rotarty Encoder Mode not Counting Properly

I am attempting to use a rotary encoder (Bourns PEC11R-4215F-S0024) with an STM32F091 Nucleo board. I would like to have it count a consist number of "counts" for every "click" of the encoder.Hardware Setup: Pin A is connected to PA0, Pin B is connec...

NicholasYunker_2_0-1688216352254.png NicholasYunker_2_1-1688216352101.png

STM32F4 Resetting itself (Nucleo 64)

Posted on April 14, 2017 at 00:58Hi!I have a Nucleo64-446RE and every 5/10 minutes the board resets itself.I'm using the Virtual COM to send data to my PC and plot it (among many other things), and when the board resets I lose the Serial connection....

0690X00000606kYQAQ.png 0690X00000606llQAA.png

Flashing STM32 with hyper terminal using inbuilt bootloader

Hi,I was flashing the STM32 Nulceo_h723zg which is having inbuilt primary bootloader in STMCube programmer, by making BOOT pin high via UART.But i want to flash by using hyper terminals like teraterm. How can we send binary or hex files into stm boar...

rsh.1 by Associate II
  • 9724 Views
  • 10 replies
  • 0 kudos