cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32F767ZI support Battery charging detection (BCD)?

ŁJura.1
Associate II

Hello team!

I am newbie in STM32 world so probably i am missing something but please clarify this for me. I have found conficting informations:

  • Datasheet "DS11532 Rev 7" at p. 47 says "Battery Charging Specification Revision 1.2 support"
  • Reference Manual "RM0410 Rev 4", p. 1579 - "supports charging port detection as described in Battery Charging Specification Revision 1.2 on the FS PHY transceiver only."
  • the same manual at p. 1638 describes registers related to BCD functionality

however:

  • the same manual again says at p. 1581 that this MCU doesn't support BCD at all
  • there are no BCD related functions in stm32f7xx_hal_pcd_ex files
  • there are no BCD related registers in stm32f767xx.h file

so i am little bit confused about that.

BR.

Lukasz

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @ŁJura.1 ,

 

The STM32F76xxx and STM32F77xxx doesn't support battery charging detection (BCD).

 

I confirm the issue and I reported Internally.

 

Internal ticket number: 147085 (This is an internal tracking number and is not accessible or usable by customers).

 

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

 

Thank you.  

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KDJEM.1
ST Employee

Hello @�?ukasz Juraszek​ and welcome to the community :smiling_face_with_smiling_eyes:,

Thank you for reporting this issue.

I confirm this confusion and I will check internally.

I will get back to you as soon as possible. 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hi @ŁJura.1 ,

 

The STM32F76xxx and STM32F77xxx doesn't support battery charging detection (BCD).

 

I confirm the issue and I reported Internally.

 

Internal ticket number: 147085 (This is an internal tracking number and is not accessible or usable by customers).

 

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

 

Thank you.  

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.