STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bluepill to STM32F446 with CAN Bus

Hi. I have developed a CAN based protocol to a Bluepill and now I need to test that on the Nucleo board as well. I have been trying this for a while now and for some reason CAN messages are generated from the Nucleo board. The code was working fine w...

Resolved! STM32L4+ and W25Q QSPI weird problem

Hi guys,Currently i am trying to get QSPI W25Q512 working correctly with STM32L4R9 but weird thing happened.I am able to write data to the memory but if i start with address 0u i get data somehow shifted by 1u. For example the array of test data star...

Eiffel by Senior
  • 2931 Views
  • 3 replies
  • 0 kudos

Resolved! FLASH_PageErase() works but HAL_FLASHEx_Erase() does not

SOLVED:  I didn't convert the flashErase_handle.PageAddress to hex, so I was passing in the integer 800_8000, which is much less than 0x800_8000I'm using the Nucleo F303RE board and as part of a bootloader trying to erase pages of flash containing th...

How to enable only M7 core on dual processor MCU.

Hi, I have a STM32H745 MCU, which has both M7 core and M4 core. I created a project in CubeIDE, and the code that is automatically generated expects both processors to be active.Indeed, in the code of the main. of core M7, wait for core M4 to boot be...

FMass.1 by Associate III
  • 2245 Views
  • 2 replies
  • 0 kudos