cancel
Showing results for 
Search instead for 
Did you mean: 

How do i free up boot0 pin to use sai with mastrclk? datasheet is not clear I'm using stm32g473cct3

TMich.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @TMich.1​ 

According to the datasheet STM32G473xB (DS12712 Rev 4), the SAI1_MCLK_A alternate function is available on PA3 as well for devices in the LQFP48 package.

Hope this helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

1 REPLY 1
FBL
ST Employee

Hello @TMich.1​ 

According to the datasheet STM32G473xB (DS12712 Rev 4), the SAI1_MCLK_A alternate function is available on PA3 as well for devices in the LQFP48 package.

Hope this helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL