STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 general VLAN handling not working as described

I am currently implementing a Profinet protocol on the STM32H743 which needs VLAN information in some packet types. Since the VLAN tags are already generated by the software for transmit packets I tried to get these tags passed through the Ethernet M...

JMH by Associate II
  • 4916 Views
  • 2 replies
  • 2 kudos

Resolved! Nucleo-H755ZI-Q not detected by usb

Hi thereI bought two Nucleo-H755ZI-Q (NUH755ZIQ$AT3) boards.Non of them show up as USB devices on either of my computers.I have tried connecting through the IDE 1.13.1; STLinkUpgrade  3.12.3 and the newest cubeprogrammer. neither can find the device....

JOKH by Associate
  • 6360 Views
  • 3 replies
  • 2 kudos

STM32H745 LTDC Interface

Dear STM community,We are using a STM32H745 microcontroller interface with 1280 x800 TFT lvds display.RGB data from controller LTDC data convert through SN75LVDS83 ic and LVDS data fed to tft display.we are facing a issue in pixel format which is not...

D6 by Associate
  • 2295 Views
  • 1 replies
  • 0 kudos

STM32 with usb HUB and multiple STM32 devices

Hi,I been trying to set up a stm32F405 mcu usb host with a hub onto which 4x stm32 device is connected. I would use these 4 devices to send data to the main mcu periodicaly at 50Hz, and to have the data transfer syncronised from the 4 devices to be o...

RBacs.1 by Associate II
  • 15467 Views
  • 10 replies
  • 0 kudos

MCU is reset when wake up from standby-dstandby

We are working with STM32H7-Disco (Dual Core). Can we only wakeup M4 core and put the system in dstandby1 mode.I mean, if we are in Standby mode and we use a tamper interrupt from a button, our system reset M7 core and M4 core, but we want only wakeu...

CBraojos by Associate II
  • 3938 Views
  • 6 replies
  • 0 kudos

detect standby wake up RTC or Reset button stm32f401

Hi,This is my first post by the way, I do have stm32f401 and I am trying to use the stand by mode , I want to detect the wakeup reason, is it RTC or reset button, in case of RTC I will do one thing and incase of reset button I will do something else,...

UART on STM32F091 stops receiving data even if they're sent

So, I'm having strange behavior regarding the serial number of my board with an STM32F091.I have a Python software that sends a packet on the serial port every 100 ms. I have initialized the serial port on the ucontroller with the same settings as ar...

nico23 by Senior III
  • 4332 Views
  • 1 replies
  • 2 kudos

Resolved! stm32h747-disco BSP problems

Hello;I have the STM32H747I-DISCO card CPN: STM32H747I-DISCO, FG: DK32H747/SAT1, and on the MB1166-A03 screen A225300631. The problem is when I try to test the card with the BSP example, I encounter the following problem:I saw in the forums regarding...

Kfell1_0-1694361566801.png
Kfell.1 by Associate III
  • 11330 Views
  • 18 replies
  • 0 kudos