STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 mute mode using address mark detection

I am using STM32L4P5 or STM32L4R9 microcontrollers and want to implement multiple-processor serial communication with 9-bit data length.As indicated by the following picture from the RM0432 reference manual, MCU will go into normal when address bit( ...

Denny007_0-1694724448466.png
Denny007 by Associate
  • 3380 Views
  • 1 replies
  • 0 kudos

STM32CO11 DELAYS NOT WORKING

  if(Mains>0.1) { if((Mains<1) &&(Vbat>0.9)) { TIM1->CCR4=TIM1->ARR; HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_4); Set_LED(0); Batt_Chrge(0); HAL_Delay(1...

meena by Associate III
  • 1025 Views
  • 2 replies
  • 0 kudos

Resolved! CHOOSE MCU

Hi.I work on BMS. I want a master-slave topology. I want to use 300 slave cards and 1 master card. This BMS is for automotive. I check ST MCU. I guess, The card should be 10-bit I2C. Because I want 300 Slave cards. So, Can you Help me this subject? W...

bngstskn by Associate III
  • 4007 Views
  • 9 replies
  • 7 kudos

GPIO HAL pointer at function argument

Hi, i m reading the general HAL GPIO file, what does the 2 pointers here do? can anyone kindly advise? i see a lot of STM header and device file with these... void HAL_GPIO_Init(GPIO_TypeDef *GPIOx, GPIO_InitTypeDef *GPIO_Init){uint32_t position = 0x...

Using Input captur in PWM mode with DMA

Hello, I want to capture the duty cycle of an input PWM with the timer feature PWM Input on CH1.Channel 1 is configured on rising edge, channel 2 is configured on falling edge.The DMA is configured for this timer on channel 1, channel 2 can't have DM...

I2.1 by Associate II
  • 5080 Views
  • 5 replies
  • 0 kudos

Resolved! L431 Stops working after enabling ADC

Hello all,I recently ran into this problem where the MCU would instantly stop working after enabling the DAC. The behavior is that from the debug view of STM32IDE the program is still running, but all variable values are reset to 0, and once the prog...

ZJing_0-1694859495061.png
ZJing by Associate III
  • 3843 Views
  • 5 replies
  • 3 kudos

Resolved! I don't know how to use the stm32 extension package.

Hello.I am a college student who is using cortex for the first time.I downloaded stm32cube expansion from stm32 and downloaded format is exe file.I downloaded these exe files and installed them on my computer, but there was a problem from here.I down...

Koseo.1 by Associate II
  • 5056 Views
  • 8 replies
  • 0 kudos

32F417 IWDG - hardware watchdog mode question

If you set the IWDG to start using the option byte, the watchdog cannot be disabled subsequently. Am I right thata) the prescaler can be modifiedb) the counter itself can be reloadedItem b) would be a vulnerability, surely, because faulty code could ...

PHolt.1 by Senior III
  • 4657 Views
  • 3 replies
  • 0 kudos