STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G030 burns itself when power up

I soldered a stm32g030F6P6 on ssop-to-beadboard PCB. When I connect Vdd(pin4) to 3V, Vss(pin5) to ground it will over current and burn it self (about 200mA input current). I have burnt 3 of it.I find out that the input resistance of power rail is sup...

IMG20231001233312.jpg

Resolved! Complementary PWM output generation with DMA

Hello Team,I'm working with complementary pwm generation with DMA, but I'm not able to generate the complementary output, but it is working fine with without DMA, please provide me the solution to proceed further.  Please find my attached source code...

STM32U5 low power audio with I2S

Hello,I'm looking into the STM32U5 for an audio application.I have a microphone that works with I2S and I want to use it with the STM32U5 in a power efficient way.I've seen that the SAI peripheral can with with I2S but it can't stay on during STOP mo...

GG.2 by Associate II
  • 4481 Views
  • 3 replies
  • 1 kudos

Resolved! Solution to avoid immediate TIM IRQ in CMSIS.

Hi,I 'm trying to code TIM to count 5s for me using CMSIS. Using the code snippet provided below I got IRQ immediately.RCC->APBENR2 |= RCC_APBENR2_TIM16EN ; // Enable TIM16 clock TIM16->PSC = 16000 - 1 ; // 1 ms TIM16->ARR = 10000 - 1 ; // 10 s = 100...

STM32F2XX + SDIO + FatFs problem

Posted on January 09, 2012 at 10:38Hi, I've a problem with my STM32. I need to use fat filesystem on SD card to read/write/create files. I tried to use Chan FatFs module but it didn't working at all ... I use SD card in SDIO and 4 wires mode. When I...

Resolved! Voltage Regulator in STM32H7 HAL Manual

Hi,I just wanted to mention that its really frustrating that in the STM32H7 HAL Manual, in the RCC Section,1. There isnt a simple step by step guide to setting up the clock config to follow along, like there is for other things like GPIO's. As someon...