STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SystemClock_Config() fails with some clock rates

I'm trying a simple blinking LED on a STM32H743VIT6 with STM32CubeIDE 1.13.2, using the clock configuration wizard. When the clock rate is set to 90MHz everything is fine, but at 480MHz the program cannot get past the SystemClock_Config() call. When ...

iforce2d by Associate III
  • 2509 Views
  • 3 replies
  • 1 kudos

STM32F103RCT6 - BusFault on address 0x20010000

Hi all,I'm trying to debug a bus fault that happen on a region on ram that is not supposed to exists. MCU has 48kb of RAM, so start from 0x20000000 to 0x2000C000, but i'm able to write 0xFF from 0x2000C000 to 0x20010000.. why??I can see also some dat...

rdzdvd_0-1696414700487.png
rdzdvd by Associate II
  • 4698 Views
  • 4 replies
  • 0 kudos

System bootloader

Hello,I'm currently working on a system bootloader using an STM32L4P5VGTx board. During this process, the board entered an unknown state and doesn't seem to recover even after a reset.I also attempted to use the Cube Programmer tool to load a bin fil...

pvall.1 by Associate II
  • 1213 Views
  • 1 replies
  • 0 kudos

Not expected frequency on NUCLEO-L496 RTC output calibration

Hi,I'm trying to improve the accuracy of RTC. For that, I use the AN2604 witch describe this.But, when I activate the calibration output of RTC at 512Hz, I have only 496Hz at the output. (AsynchPrediv =127). I tried this simple code to the nucleo-L47...

Sirac by Associate III
  • 3891 Views
  • 8 replies
  • 0 kudos

''unknown device'' error in ST Link Utility

Posted on November 27, 2015 at 10:52When I try to target->connect in ST Link Utility I have an error ''unknown device'' with disco L4, disco F7 and nucleo L4. With nucleo L0, the connection is good, but I have the message ''Device family : unknown d...

SPI Clock rate limitation?

TL;DR. What are the limiting factors for incoming clock speed for an SPI peripheral operating in slave mode?I'm using the STM32U575 MCU with a few peripherals, and am clocking it down to 16MHz for SYSCLK and all related peripherals.  I'm generating a...

sethkaz by Associate III
  • 13492 Views
  • 15 replies
  • 3 kudos