STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Determining Motor Position using one Hall Signal

Hello,I am using the stm32f042k6t6 to control a Motor which has one Hall Signal. The motor is connected to a Jack which I drive in clockwise and anticlockwise direction, so in and out. The jacks start at a specific position and I want that when I dri...

Resolved! Help implementing SPI using just registers

Hello everyone,I am having trouble communicating with CC1101 radio SPI slave. With HAL, the transfers work well and I am able to read every register, but because I am using stm32f042 MCU, I'm low on flash memory because I'm also using USB CDC. So I'm...

LLope.31 by Associate III
  • 4461 Views
  • 4 replies
  • 1 kudos

STM32U585 RTOS - Threadx - PSA certification

Hello team,Greetings!We have selected Trust zone MCU STM32U585ZIT6Q (U5 series) for our product (EV charger) development.We planned to use STM32 inbuilt 'Threadx' OS as RTOS for our product FW development. Could you confirm, is this PSA certified? Al...

Siva1 by Associate
  • 947 Views
  • 0 replies
  • 0 kudos

Resolved! EOT to early

Hi.implementing a SPI master (NOT using HAL) with software based SS i am searching for the right way to detect the end of a transmission to release the SS again.EOT (in SPI_SR) gets set when the last Bit is is set to the MOSI Lane. --> so this is too...

dbahr by Associate II
  • 3774 Views
  • 8 replies
  • 0 kudos

Resolved! 32kB flash overflowing using just USB CDC and SPI

Hello everyone,I am trying to use both USB CDC and SPI on a STM32F042F6P6 MCU. Unfortunately, without even writing almost any code (just an HAL_SPI_TransmitReceive() and a CDC_Transmit_FS()) it says the flash memory overflows by 1484 bytes.Is this no...

LLope.31 by Associate III
  • 2719 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE not flashing MCU

Hi! I'm trying to flash a STM32L422KBT6 with STM32CubeIDE 1.13.2 and ST-LINK V2 and I keep getting this error: Error: failed to erase memoryEncountered Error when opening C:\ST\STM32CubeIDE_1.13.2\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externa...