Associate II
Dec 14, 2020 1:20 PM UTC
Solved
Using both CAN1 & CAN2 both in STM32F446RC
- 10 replies
- 6404 views
Hi, I want to use both CAN1 and CAN2 for my application with 500kbps and 125kbps speeds respectively. I have initialized both of them as per my requirements using HAL. Where in Tx is implemented in polling and Rx in interrupts. CAN1 Tx and Rx working perfect. Coming to CAN2 Tx is working and Rx is not working. Interrupt itself is not firing up for CAN2 Rx (HAL_CAN_RxFifo0MsgPendingCallback is not being called). I've read in datasheet that some SRAM sharing process is happening between 2 CANs. I'm unable to comprehend that. Is that an issue?
I'm attaching the code also. Please check and help!