User Activity

Anyone have a working example of SDMMC working with an eMMC chip on the L476 or H743 series MCUs that they can share?
We have a new project and would like it to have some features similar to the STM32 on an STLink:a) Emulate a Thumbdrive using MCU FLASH and/or an external serial FLASH IC. The files should be accessible by both the STM32 and any PC connected to the U...
I'm trying to create a new module for use with TouchGFX, not an ST demo board, but our own custom PCB.TouchGFX seems to allow only creating projects for existing demo boards (nucleo, etc.). When I do this I get an ioc file, and it shows TouchGFX unde...
Sometimes I end up working on multiple branches of a project (ain't life fun!).With STM32CubeIDE it seems if I rename the project folder Project Project_Main Project_BranchXThen the Sources paths defined in the project are broken/lost, and any exclud...
We have a system of many interconnected STM32 boards of various types.Today I need to debug two identical boards of same type.I can step code in two different STM32 projects by starting two IDEs,but ...When I start multiple IDEs and try to do debug w...
Kudos from