STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_I2C_IsDeviceReady() returning HAL_BUSY

Hi, I'm using an STM32F401RE board for a class(programming using MacOS). Right now, I'm using VSCode and make to edit and compile my code, then using stlink to flash it. Now, I'm trying to communicate with an MPU6050 using I2C; however, when I run HA...

AllanLiu by Associate II
  • 9294 Views
  • 8 replies
  • 2 kudos

How to wipe the flash memory of an STM32L476RG

Hi all,I am working on a research project for my school that involves me programming a microcontroller, however, the program that I most recently flashed to my board causes the processor to quickly heat up and cause a burning smell. I am unsure if th...

STM32F103CBT6 Erase Chip using ST-Link Utility

Hi, I designed PCB including STM32F103CBT6 and I have attached schematic here as a reference. I am using SWD with an adapter from (Olimex LTD / ARM-JTAG-20-10) then connect through ST-LINK/VE debugger. After checking all voltage rails on the board, I...

shin212 by Associate II
  • 5303 Views
  • 2 replies
  • 0 kudos

SSI Slave implementation up to 10Mhz

Hi Everyone,I am  trying to implement a SSI slave for high speed applications (up to 10Mhz) on SMT32. I am not a firmware engineer and don't really have experience with this protocol. In my application, the master SSI sends the clock signal to read 4...

Jcer by Associate
  • 1902 Views
  • 0 replies
  • 0 kudos

Adding Buzzer sound in Button (TouchGfx)

I am currently using the touch gfx button with its callback function to call PWM code to execute when I press the button on the GUI as shown below.#include <main.h> #include "cmsis_os.h" extern TIM_HandleTypeDef htim4; void MAINViewBase::buttonCallb...

ZExpo.1 by Senior
  • 2552 Views
  • 3 replies
  • 2 kudos

Single AWD to monitor 2 channels from different ADCs

Hi,As from the title, is it possible to use the same AWD to monitor 2 channels from 2 different ADCs?Specifically, I have a designed a simple digitizer around a f303k8. ADC1 and ADC2 have been configured in continous mode, with AWD2 and AWD3 as monit...

STM32 for motor control, dual core MCUs?

Hello,I am looking for a solution for motor control that covers 2 applications, 1) controlling a BLDC for both spinning at constant speeds as well as stable positioning mode, and 2) driving a stepper. (sharing some hardware & software design between ...

SKled.1 by Senior II
  • 3430 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.