STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SSI Slave implementation up to 10Mhz

Hi Everyone,I am  trying to implement a SSI slave for high speed applications (up to 10Mhz) on SMT32. I am not a firmware engineer and don't really have experience with this protocol. In my application, the master SSI sends the clock signal to read 4...

Jcer by Associate
  • 1881 Views
  • 0 replies
  • 0 kudos

Adding Buzzer sound in Button (TouchGfx)

I am currently using the touch gfx button with its callback function to call PWM code to execute when I press the button on the GUI as shown below.#include <main.h> #include "cmsis_os.h" extern TIM_HandleTypeDef htim4; void MAINViewBase::buttonCallb...

ZExpo.1 by Senior
  • 2493 Views
  • 3 replies
  • 2 kudos

Single AWD to monitor 2 channels from different ADCs

Hi,As from the title, is it possible to use the same AWD to monitor 2 channels from 2 different ADCs?Specifically, I have a designed a simple digitizer around a f303k8. ADC1 and ADC2 have been configured in continous mode, with AWD2 and AWD3 as monit...

STM32 for motor control, dual core MCUs?

Hello,I am looking for a solution for motor control that covers 2 applications, 1) controlling a BLDC for both spinning at constant speeds as well as stable positioning mode, and 2) driving a stepper. (sharing some hardware & software design between ...

SKled.1 by Senior II
  • 3351 Views
  • 3 replies
  • 3 kudos

STM32G474 failed to erase chip.

I use J-Link and STM32G474, which can burn the program, but can't erase the chip. After trying to use J-Link STM to unlock the chip, it also did not work Application log started - J-Flash V7.92b (J-Flash compiled Aug 23 2023 14:00:43) - JLinkARM.dl...

kerry1 by Associate
  • 3514 Views
  • 1 replies
  • 0 kudos

HAL + FreeRTOS + FatFS Bug

Hi,We have come across a bug in the code generated if you use FreeRTOS in STATIC memory mode (rather than the default dynamic mode) , with FatFs. (All generated from the CubeMX).When we run the code we get two CONFIG ASSERTS in the RTOS and it is due...