STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change Flash Standard Boot Startup Adress with STM32ide

 using stm32ide and a stm32f407 I would like to change the boot address to 0x8000000 to leave the first 4 sectors free from 0x4000 to position the boot at 0x8010000 I made a series of settings (not sufficient). in flash.ld file change1) FLASH (rx) : ...

Resolved! STM32F411E-DISCO and MCP2515 INTERRUPT

Hello, by connecting an mcp2515 to Stm32, I enabled it to communicate properly with other cards via the Can network. However, when a message arrives, I couldn't understand how to receive it with the INT pin and I couldn't do it. I tried connecting th...

sheqom by Associate III
  • 3635 Views
  • 4 replies
  • 0 kudos

Resolved! stm32h7 lwip sdmmc1 fatfs

Hi,Is there any sample for H755 with lwip eth and sdmmc1 fatfs?.How configure the MPU region?. Thanks,    

GPHIL.1 by Associate II
  • 3042 Views
  • 3 replies
  • 0 kudos

STSPIN32G4 as 600V Version

HelloFor future blower motors in our products, we are currently using the STSPIN32F0602. Unfortunately, memory space is very limited and we would like to use the STSPIN32G4 in order to introduce new products that are as future-proof as possible. Howe...

Thomi by Associate
  • 856 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H730 ETH receive not working

Hi all,For the last couple of weeks I've been trying to deal with receiving an ETH frame from PHY on my own PCB design with STM32H730VBT.To make sure the firmware is OK I took a Nucleo-H723ZI (CPU from the same family) and configured it to work with ...

e1.png e2.png e3.png e4.png

STM32F401 I2C driver using register in Proteus simulation

I want to use two STM32F401xx MCU in proteus. One of them is to be a master and the other is to be a slave. This is my code for the master:     #include <stdint.h> #include <stdio.h> uint8_t temp=0; void begin(); void end(void); void Write (uin...

address.PNG proteus.PNG
AH25 by Associate
  • 3330 Views
  • 2 replies
  • 1 kudos

Resolved! STM32WB QSPI FLASH - Winbond(W25N01GV)

Hello,I have been trying to make a driver for the Winbond(W25N01GV)  NAND flash over QSPI but I've been failing so far. Can somebody give me some ideas about what I am doing wrong?        #define UNPACK_UINT16_TO_2_BYTES(num) {(uint8_t) (((num) & 0x...

Screenshot_45.jpg
Dracu by Associate II
  • 10694 Views
  • 7 replies
  • 3 kudos

Resolved! LAN8742A - STM32 and REF_CLK

Hi,I plan to use LAN8742A and STM32H7 for an ethernet application.In the datasheet for LAN8742A there is this very interesting sentense on page 34 i the datsheet:The REF_CLK Out Mode is not part of the RMII Specification. To ensure proper system oper...

tyassin by Associate III
  • 13648 Views
  • 9 replies
  • 3 kudos

Resolved! Running STM32H7 timers at 480Mhz

Hello, how can I get timers running at 480Mhz to have maximum resolution?Here is a capture using latest stmcube version:I have tried D2PRE1 & D2PRE2 =1 but then warnings appear

stm32.jpg
JLope.11 by Associate III
  • 6488 Views
  • 7 replies
  • 3 kudos